Hello,
I'm having the following error when trying to build for the imx8mpevk machine:
[root@fbdebian flexbuild]$ bld -m imx8mpevk
...
Setting up uidmap (1:4.13+dfsg1-1+b1) ...
Processing triggers for libc-bin (2.36-9+deb12u9) ...
I: automatically chosen mode: root
W: binfmt_misc not found in /proc/mounts -- not mounted?
E: arm64 can neither be executed natively nor via qemu user emulation with binfmt_misc
2025-02-06 01:56:44,270 bdebstrap ERROR: mmdebstrap failed with exit code 25. See above for details.
make[1]: *** [cryptodev_linux.mk:7: cryptodev_linux] Error 1
make: *** [Makefile:17: linux-modules] Error 2
Can you help me to fix it?
Thank you in advance.
I am running into the same exact problem when building using docker build option
@andreamarson I fixed the similar issue with reinstall those qemu packages, not sure why not work on your side
Please kindly refer below:
[root@fbdebian flexbuild2412]$ cat /proc/mounts
overlay / overlay rw,relatime,lowerdir=/var/lib/docker/overlay2/l/C4DWP2KVNXWKH2XJ563KJOXGXJ:/var/lib/docker/overlay2/l/3J3KTMQVPY74QGJKRPQHG727ZG:/var/lib/docker/overlay2/l/ETHHAO2WUEVEKTJZSHYP7R67PR:/var/lib/docker/overlay2/l/L22KW6O2BTJEJFRQNAYIF65I7M:/var/lib/docker/overlay2/l/5X7ZASKZL2Q4A4JPXOTXL27SUW:/var/lib/docker/overlay2/l/S5RPY5DNQMW6ARRIEVSJVMP5WT,upperdir=/var/lib/docker/overlay2/399d79f82c0e1fb6a0773eec4e1fc2353ab91d707dfbd5c0891c8eaecf407bcd/diff,workdir=/var/lib/docker/overlay2/399d79f82c0e1fb6a0773eec4e1fc2353ab91d707dfbd5c0891c8eaecf407bcd/work 0 0
proc /proc proc rw,nosuid,nodev,noexec,relatime 0 0
sysfs /sys sysfs rw,nosuid,nodev,noexec,relatime 0 0
cgroup /sys/fs/cgroup cgroup2 rw,nosuid,nodev,noexec,relatime,nsdelegate,memory_recursiveprot 0 0
udev /dev devtmpfs rw,nosuid,relatime,size=8127808k,nr_inodes=2031952,mode=755,inode64 0 0
devpts /dev/pts devpts rw,nosuid,noexec,relatime,gid=5,mode=620,ptmxmode=000 0 0
tmpfs /dev/shm tmpfs rw,inode64 0 0
hugetlbfs /dev/hugepages hugetlbfs rw,relatime,pagesize=2M 0 0
mqueue /dev/mqueue mqueue rw,nosuid,nodev,noexec,relatime 0 0
/dev/mapper/vg_data-lv_usr /usr/lib/modules ext4 rw,relatime 0 0
/dev/mapper/vg_data-lv_usr /usr/share/zoneinfo/Etc/UTC ext4 ro,relatime 0 0
/dev/mapper/vg_data-lv_home /home/nxa20322 ext4 rw,relatime 0 0
/dev/mapper/vg_data-lv_var /etc/resolv.conf ext4 rw,relatime 0 0
/dev/mapper/vg_data-lv_var /etc/hostname ext4 rw,relatime 0 0
/dev/mapper/vg_data-lv_var /etc/hosts ext4 rw,relatime 0 0
/dev/mapper/vg_data-lv_home /home/nxa20322/docker/flexbuild2412 ext4 rw,relatime 0 0
devpts /dev/console devpts rw,nosuid,noexec,relatime,gid=5,mode=620,ptmxmode=000 0 0
Thanks
@June_Lu
I have not spotted any significant difference w.r.t. to the active mounts.
Can you please send me your full log associated with the build for the machine imx8mpevk so that I can compare it with mine?
@andreamarson please try the command
sudo apt-get install qemu-system qemu-user qemu-user-static binfmt-support debootstrap binutils
I create a new file and run the command, because it depends on the ethernet link, I run other related commands first, and then run the "bld -m imx8mpevk" in the end.
See whole logs attached.
Thanks for the logs.
It is possible to related to your Host environment,
I could not reproduce the same issue.
My host is Ubuntu 22.04 host with docker.
I use the same distribution:
$ lsb_release -a
No LSB modules are available.
Distributor ID: Ubuntu
Description: Ubuntu 22.04.4 LTS
Release: 22.04
Codename: jammy
Any hint to spot where the problem could be?
To start, can you please send me the output of this command so I can see what this file should look like?
[root@fbdebian flexbuild]$ cat /proc/mounts
Is it the full logs?
Have you confirm the
Verify that the Docker installation is successful by running the hello-world image.
```
$ docker run hello-world
$ docker ps -a
docker works properly:
$ docker run hello-world
Hello from Docker!
This message shows that your installation appears to be working correctly.
To generate this message, Docker took the following steps:
1. The Docker client contacted the Docker daemon.
2. The Docker daemon pulled the "hello-world" image from the Docker Hub.
(amd64)
3. The Docker daemon created a new container from that image which runs the
executable that produces the output you are currently reading.
4. The Docker daemon streamed that output to the Docker client, which sent it
to your terminal.
To try something more ambitious, you can run an Ubuntu container with:
$ docker run -it ubuntu bash
Share images, automate workflows, and more with a free Docker ID:
https://hub.docker.com/
For more examples and ideas, visit:
https://docs.docker.com/get-started/
amarson@LW11Y24037:~/devel/dsab/sw/linux/RTK0EF0177Z00002ZJ-v1.0.1$ docker ps -a
CONTAINER ID IMAGE COMMAND CREATED STATUS PORTS
NAMES
bb81ea6a0099 hello-world "/hello" 9 seconds ago Exited (0) 7 seconds ago
distracted_roentgen
503a17e14c01 fbdebian:12 "/bin/bash" 40 hours ago Up 40 hours
amarson_fbdebian_12_555c33
07080445a948 excalidraw/excalidraw:latest "/docker-entrypoint.…" 3 days ago Up 3 days (healthy) 0.0.0.0:5000->80/tcp, :::5000->80/tcp excalidraw
1bdbc6826aaf budibase/proxy "/docker-entrypoint.…" 7 months ago Exited (0) 7 months ago
bbproxy
b1777d09ad35 budibase.docker.scarf.sh/budibase/apps "docker-entrypoint.s…" 7 months ago Exited (137) 7 months ago
bbapps
07d6b116ab00 budibase.docker.scarf.sh/budibase/worker "docker-entrypoint.s…" 7 months ago Exited (137) 7 months ago
bbworker
2ff233a6bd39 redis "docker-entrypoint.s…" 7 months ago Exited (0) 7 months ago
budibase-docker-redis-service-1
267066eea7a5 budibase/couchdb "tini -- /docker-ent…" 7 months ago Exited (143) 7 months ago
budibase-docker-couchdb-service-1
40a3b1a5ae01 containrrr/watchtower "/watchtower --debug…" 7 months ago Up 3 days (healthy) 8080/tcp
budibase-docker-watchtower-service-1
950529d1adc7 minio/minio "/usr/bin/docker-ent…" 7 months ago Exited (0) 7 months ago
budibase-docker-minio-service-1
8cdb5e08ba8c nodered/node-red "./entrypoint.sh" 7 months ago Exited (130) 7 months ago
mynodered2
82aa692ee66a nodered/node-red "./entrypoint.sh" 7 months ago Exited (130) 7 months ago
mynodered
e072a885ce2b hello-world "/hello" 8 months ago Exited (0) 8 months ago
stupefied_fermat
1833397a90b8 hello-world "/hello" 8 months ago Exited (0) 8 months ago
zen_chaum
I'll attach the full log too.