failing `bitbake oem-deere-display-image -c populate_sdk_ext`

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

failing `bitbake oem-deere-display-image -c populate_sdk_ext`

485 Views
TimNew
Contributor I

I am having issues building the esdk. I am getting the following error

You can also run generated qemu images with a command like 'runqemu qemux86-64'.

Other commonly useful commands are:
- 'devtool' and 'recipetool' handle common recipe tasks
- 'bitbake-layers' handles common layer tasks
- 'oe-pkgdata-util' handles common target package tasks
ERROR: bitbake failed:
WARNING: You are using a local hash equivalence server but have configured an sstate mirror. This will likely mean no sstate will match from the mirror. You may wish to disable the hash equivalence use (BB_HASHSERVE), or use a hash equivalence server alongside the sstate mirror.
WARNING: You are using a local hash equivalence server but have configured an sstate mirror. This will likely mean no sstate will match from the mirror. You may wish to disable the hash equivalence use (BB_HASHSERVE), or use a hash equivalence server alongside the sstate mirror.
Loading cache...done.
Loaded 0 entries from dependency cache.
Parsing recipes...done.
ERROR: No recipes in default available for:
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-freescale/recipes-graphics/vulkan/vulkan-loader_1.2.182.0.bbappend
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-atf/imx-atf_%.bbappend
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-mkimage/imx-boot_1.0.bbappend
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-mkimage/imx-mkimage_git.bbappend
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/scfw-deere-display/imx-sc-firmware_%.bbappend
No recipes in ngpd2 available for:
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-freescale/recipes-graphics/vulkan/vulkan-loader_1.2.182.0.bbappend
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-atf/imx-atf_%.bbappend
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-mkimage/imx-boot_1.0.bbappend
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-mkimage/imx-mkimage_git.bbappend
/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/sdk-ext/image/tmp-renamed-sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/scfw-deere-display/imx-sc-firmware_%.bbappend
Parsing of 5594 .bb files complete (0 cached, 5594 parsed). 8682 targets, 1176 skipped, 0 masked, 0 errors.

Summary: There were 2 WARNING messages.
Summary: There was 1 ERROR message, returning a non-zero exit code.
ERROR: Logfile of failure stored in: /workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/temp/log.do_populate_sdk_ext.101435
ERROR: Task (/workdir/sources/openembedded-core/../meta-deere-oem/meta-oem/recipes-core/images/oem-deere-display-image.bb:do_populate_sdk_ext) failed with exit code '1'
Pseudo log:
path mismatch [8 links]: ino 28324762 db '/workdir/build-ngpd2/tmp/work/ngpd2-deere-linux/oem-deere-display-image/1.0-r0/rootfs/usr/share/common-licenses/imx-gpu-viv/EULA' req '/workdir/sources/meta-freescale/EULA'.
Setup complete, sending SIGUSR1 to pid 101436.

NOTE: Tasks Summary: Attempted 3900 tasks of which 3898 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/workdir/sources/openembedded-core/../meta-deere-oem/meta-oem/recipes-core/images/oem-deere-display-image.bb:do_populate_sdk_ext
Summary: There were 2 WARNING messages.
Summary: There were 2 ERROR messages, returning a non-zero exit code.

0 Kudos
Reply
0 Replies