failed to get SDK after executing bitbake imx-image-core -c populate_sdk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

failed to get SDK after executing bitbake imx-image-core -c populate_sdk

2,199件の閲覧回数
DarrenJi
Contributor I

Hi all:

I tried to get SDK and image as <i.MX Yocto Project User's Guide Rev. L5.4.47_2.2.0 > and get image successfully, but get error as below when I move on to get SDK.

any idea on fix it?

WARNING: Host distribution "ubuntu-20.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache...done.
Loaded 4623 entries from dependency cache.
Parsing recipes...done.
Parsing of 3209 .bb files complete (3208 cached, 1 parsed). 4624 targets, 252 skipped, 1 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION           = "1.44.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "ubuntu-20.04"
TARGET_SYS           = "aarch64-poky-linux"
MACHINE              = "imx8dxlevk"
DISTRO               = "fsl-imx-xwayland"
DISTRO_VERSION       = "5.4-zeus"
TUNE_FEATURES        = "aarch64"
TARGET_FPU           = ""
meta                
meta-poky           
meta-oe             
meta-multimedia     
meta-python         
meta-freescale      
meta-freescale-3rdparty
meta-freescale-distro
meta-bsp            
meta-sdk            
meta-ml             
meta-nxp-demo-experience = "<unknown>:<unknown>"
meta-browser         = "HEAD:ee3be3b5986a4aa0e73df2204a625ae1fe5df37e"
meta-rust            = "<unknown>:<unknown>"
meta-clang           = "HEAD:711e593d5984aad3bf35c51b7ac4482982bc16c7"
meta-gnome          
meta-networking     
meta-filesystems    
meta-qt5            
meta-python2         = "<unknown>:<unknown>"
Initialising tasks...done.
Sstate summary: Wanted 157 Found 0 Missed 157 Current 1354 (0% match, 89% complete)
NOTE: Executing Tasks
NOTE: Setscene tasks completed
NOTE: Running task 2571 of 5123 (virtual:native:/home/ubuntu/Documents/yocto/imx-yocto-bsp/sources/meta-clang/recipes-devtools/clang/clang_git.bb:do_compile)
NOTE: recipe clang-native-9.0.1-r0: task do_compile: Started
NOTE: Running task 3125 of 5123 (/home/ubuntu/Documents/yocto/imx-yocto-bsp/sources/poky/meta/recipes-devtools/binutils/binutils-cross-canadian_2.32.bb:do_compile)
NOTE: recipe binutils-cross-canadian-aarch64-2.32.0-r0: task do_compile: Started
NOTE: Running task 3467 of 5123 (virtual:nativesdk:/home/ubuntu/Documents/yocto/imx-yocto-bsp/sources/poky/meta/recipes-devtools/perl/perl_5.30.1.bb:do_compile)
NOTE: Running task 3668 of 5123 (virtual:nativesdk:/home/ubuntu/Documents/yocto/imx-yocto-bsp/sources/poky/meta/recipes-devtools/qemu/qemu_4.1.0.bb:do_compile)
NOTE: recipe nativesdk-perl-5.30.1-r0: task do_compile: Started
ERROR: nativesdk-perl-5.30.1-r0 do_compile: oe_runmake failed
ERROR: nativesdk-perl-5.30.1-r0 do_compile: Execution of '/home/ubuntu/Documents/yocto/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-perl/5.30.1-r0/temp/run.do_compile.52536' failed with exit code 1:
make: *** No targets specified and no makefile found.  Stop.
WARNING: exit code 1 from a shell command.
ERROR: Logfile of failure stored in: /home/ubuntu/Documents/yocto/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-perl/5.30.1-r0/temp/log.do_compile.52536
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 8
| make: *** No targets specified and no makefile found.  Stop.
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '/home/ubuntu/Documents/yocto/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/nativesdk-perl/5.30.1-r0/temp/run.do_compile.52536' failed with exit code 1:
| make: *** No targets specified and no makefile found.  Stop.
| WARNING: exit code 1 from a shell command.
|
NOTE: recipe nativesdk-perl-5.30.1-r0: task do_compile: Failed
ERROR: Task (virtual:nativesdk:/home/ubuntu/Documents/yocto/imx-yocto-bsp/sources/poky/meta/recipes-devtools/perl/perl_5.30.1.bb:do_compile) failed with exit code '1'
NOTE: recipe nativesdk-qemu-4.1.0-r0: task do_compile: Started
ERROR: binutils-cross-canadian-aarch64-2.32.0-r0 do_compile: oe_runmake failed
ERROR: binutils-cross-canadian-aarch64-2.32.0-r0 do_compile: Execution of '/home/ubuntu/Documents/yocto/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/binutils-cross-canadian-aarch64/2.32.0-r0/temp/run.do_compile.52487' failed with exit code 1:
make[1]: Entering directory '/home/ubuntu/Documents/yocto/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/binutils-cross-canadian-aarch64/2.32.0-r0/git/build.x86_64-pokysdk-linux.aarch64-poky-linux'
make[1]: Nothing to be done for 'all-target'.
make[2]: Entering directory '/home/ubuntu/Documents/yocto/imx-yocto-bsp/build/tmp/work/x86_64-nativesdk-pokysdk-linux/binutils-cross-canadian-aarch64/2.32.0-r0/git/build.x86_64-pokysdk-linux.aarch64-poky-linux/intl'

 

 

0 件の賞賛
返信
1 返信

1,464件の閲覧回数
Rgulde
Contributor III

Was a solution found? The log indicates Ubuntu /focal/ version 20.04 not tested?

0 件の賞賛
返信