fail to mount ( rw option, type 1DX... )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fail to mount ( rw option, type 1DX... )

922 Views
openclosed
Contributor I

I purchased the i.MX6QP SABRE Board.
Here is an SD card with Android porting.
And I want to connect murata type 1dx wifi module to i.MX6qp saber.
The murata guide document says to copy the Type 1DX firmware to the "/etc/firmware/bcm" folder.
However, the "/etc/firmware/bcm" folder is "read only" and cannot be copied.


So I did the mount command.
sabresd_6dq: / # mount -o rw, remount / system
However, with the following error, "rw" was not an option.

Buffer I / O error on dev dm-0, logical block 0, lost sync page write
EXT4-fs (dm-0): re-mounted. Opts: data = ordered
sabresd_6dq: / #
sabresd_6dq: / # Buffer I / O error on dev dm-0, logical block 360954, lost sync page write
JBD2: Error -5 detected when updating journal superblock for dm-0-8.
Aborting journal on device dm-0-8.
Buffer I / O error on dev dm-0, logical block 360954, lost sync page write
JBD2: Error -5 detected when updating journal superblock for dm-0-8.

Why does this happen?
 Is there any way to copy Type 1DX firmware to "/etc/firmware/bcm" folder?

0 Kudos
2 Replies

833 Views
igorpadykov
NXP Employee
NXP Employee

Hi An

one can try steps using latest rev.6 Murata Guide

https://wireless.murata.com/pub/RFM/data/murata_quick_start_guide_linux.pdf 

http://static6.arrow.com/aropdfconversion/bc3c28c948475b6addee41fdba542e876dcb5527/murata_quick_star... 

also may be useful to post issue on

Space: Murata | Cypress Developer Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

833 Views
openclosed
Contributor I

Hi. igorpadykov


Thank you very much for answering my question.
I have seen Linux, Android guide documentation.
Since copying files to / system folder is a phenomenon of i.mx
You may be able to answer here.
Do you know why there is a problem mounting?

0 Kudos