fail to compile yocto (imx-3.14.38-6QP_ga)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

fail to compile yocto (imx-3.14.38-6QP_ga)

2,058 次查看
wangzhigang
Contributor III

hi,everyone

we compile the yocto imx-3.14.38-6QP_ga for wayland.

My PC env is :

ubuntu 14.04

DDR 32GB(enough memory)

MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-wayland -e wayland

bitbake fsl-image-qt5

when the yocto compile the qtwebengine,we get the error as follow:

make[3]: Entering directory `/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtwebengine/5.4.2+gitAUTOINC+qtwebengine-r0/git/src/core'

rm -f libQt5WebEngineCore.so.5.4.3 libQt5WebEngineCore.so libQt5WebEngineCore.so.5 libQt5WebEngineCore.so.5.4

linking ../../lib/libQt5WebEngineCore.so.5.4.3

/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/sysroots/i686-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.9.2/ld: failed to set dynamic section sizes: Memory exhausted

collect2: error: ld returned 1 exit status

make[3]: *** [../../lib/libQt5WebEngineCore.so.5.4.3] Error 1

make[3]: Leaving directory `/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtwebengine/5.4.2+gitAUTOINC+qtwebengine-r0/git/src/core'

make[2]: *** [sub-core_module-pro-make_first] Error 2

make[2]: Leaving directory `/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtwebengine/5.4.2+gitAUTOINC+qtwebengine-r0/git/src/core'

make[1]: *** [sub-core-make_first] Error 2

make[1]: Leaving directory `/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtwebengine/5.4.2+gitAUTOINC+qtwebengine-r0/git/src'

make: *** [sub-src-make_first] Error 2

how can I solove the problem,or how to remove the qtwebengine module,I remove the file sources/meta-qt5/recipes-qt/qt5/qtwebengine_git.bb,but it doesn't work.

Please give me a handle.

Best Regards.

标记 (1)
0 项奖励
回复
2 回复数

1,349 次查看
igorpadykov
NXP Employee
NXP Employee

Hi wang

that release was tested only on QP processor, please use latest

consolidated for all processors L3.14.52 release:

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,350 次查看
wangzhigang
Contributor III

hi,igor

thanks for your replay,do you have some doc for compile wayland independent,because we found the yocto binding the  qt5 version.we just want to use qt5.4 + wayland in imx6q.so we plan to compile wayland independent.

0 项奖励
回复