fail to compile yocto (imx-3.14.38-6QP_ga)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fail to compile yocto (imx-3.14.38-6QP_ga)

2,240 Views
wangzhigang
Contributor III

hi,everyone

we compile the yocto imx-3.14.38-6QP_ga for wayland.

My PC env is :

ubuntu 14.04

DDR 32GB(enough memory)

MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-wayland -e wayland

bitbake fsl-image-qt5

when the yocto compile the qtwebengine,we get the error as follow:

make[3]: Entering directory `/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtwebengine/5.4.2+gitAUTOINC+qtwebengine-r0/git/src/core'

rm -f libQt5WebEngineCore.so.5.4.3 libQt5WebEngineCore.so libQt5WebEngineCore.so.5 libQt5WebEngineCore.so.5.4

linking ../../lib/libQt5WebEngineCore.so.5.4.3

/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/sysroots/i686-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.9.2/ld: failed to set dynamic section sizes: Memory exhausted

collect2: error: ld returned 1 exit status

make[3]: *** [../../lib/libQt5WebEngineCore.so.5.4.3] Error 1

make[3]: Leaving directory `/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtwebengine/5.4.2+gitAUTOINC+qtwebengine-r0/git/src/core'

make[2]: *** [sub-core_module-pro-make_first] Error 2

make[2]: Leaving directory `/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtwebengine/5.4.2+gitAUTOINC+qtwebengine-r0/git/src/core'

make[1]: *** [sub-core-make_first] Error 2

make[1]: Leaving directory `/home/pm/fsl-arm-yocto-bsp-3.14.38-6QP_ga/build-wayland/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtwebengine/5.4.2+gitAUTOINC+qtwebengine-r0/git/src'

make: *** [sub-src-make_first] Error 2

how can I solove the problem,or how to remove the qtwebengine module,I remove the file sources/meta-qt5/recipes-qt/qt5/qtwebengine_git.bb,but it doesn't work.

Please give me a handle.

Best Regards.

Tags (1)
0 Kudos
Reply
2 Replies

1,531 Views
igorpadykov
NXP Employee
NXP Employee

Hi wang

that release was tested only on QP processor, please use latest

consolidated for all processors L3.14.52 release:

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,532 Views
wangzhigang
Contributor III

hi,igor

thanks for your replay,do you have some doc for compile wayland independent,because we found the yocto binding the  qt5 version.we just want to use qt5.4 + wayland in imx6q.so we plan to compile wayland independent.

0 Kudos
Reply