error not build .mk file completely in imx8mm android OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error not build .mk file completely in imx8mm android OS

938 Views
Ruban1
Contributor II

i have editted in dts file and tried to build kernel

Error in file inside device

UbootKernelBoardConfig.mk

till u boot is getting build properly

# u-boot target used by uuu for imx8mm_evk with DDR4 on board
TARGET_BOOTLOADER_CONFIG += imx8mm-ddr4-evk-uuu:imx8mm_ddr4_evk_android_uuu_defconfig
# u-boot target used by uuu for imx8mm_evk with LPDDR4 on board
TARGET_BOOTLOADER_CONFIG += imx8mm-evk-uuu:imx8mm_evk_android_uuu_defconfig
TARGET_BOOTLOADER_CONFIG += imx8mm-4g-evk-uuu:imx8mm_evk_4g_android_uuu_defconfig

After this only the error starts and comes out of the loop.It doesnt mention any error

Its not able to get into the next line

# imx8mm kernel defconfig
TARGET_KERNEL_DEFCONFIG := imx_v8_android_defconfig
TARGET_KERNEL_ADDITION_DEFCONF := android_addition_defconfig

Labels (1)
0 Kudos
Reply
1 Reply

893 Views
b36401
NXP Employee
NXP Employee
0 Kudos
Reply