When I run directfb sample df_sok, I got this error msg below, can anyone help? thanks.
I'm using imx6q board, and build from latest ltib without any problem.
root@freescale /$ df_dok
~~~~~~~~~~~~~~~~~~~~~~~~~~| DirectFB 1.4.0 |~~~~~~~~~~~~~~~~~~~~~~~~~~
(c) 2001-2009 The world wide DirectFB Open Source Community
(c) 2000-2004 Convergence (integrated media) GmbH
----------------------------------------------------------------
(*) DirectFB/Core: Single Application Core. (2014-02-04 07:39)
(*) Direct/Memcpy: Using libc memcpy()
:smileyalert: DirectFB/core/vt: Couldn't open neither `/dev/tty0' nor `/dev/vc/0'!
--> No such file or directory
:smileyalert: DirectFB/Core: Could not initialize 'system_core' core!
--> Initialization error!
df_dok.c <1457>:
(#) DirectFBError [DirectFBCreate( &dfb )]: Initialization error!
root@freescale /$
 
					
				
		
Yifei
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
 
					
				
		
Yifei
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel
free to reply with an update to this discussion.
Thanks,
Yixing
 Bio_TICFSL
		
			Bio_TICFSL
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Did you try df_dok - - dfb:no-vt, if this doesn't work check the full debug trace 
 
 $> df_dok --dfb:debug
Also, you may need to compile the Linux Kernel with "Virtual terminal". You can find this option under Device Drivers ---> Character Devices ---> Virtual terminal.
Hope this helps