Hi,
I am getting the below error for the Phy IC DP83848 in RMII Mode in IMX8MMini
Error: ethernet@30be0000 address not set.
Below is the uboot log
-------------------------------------------------------------------------------------------
switch to partitions #0, OK
mmc1(part 0) is current device
flash target is MMC:1
Net:
Error: ethernet@30be0000 address not set.
No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 2 1 0
switch to partitions #0, OK
mmc1(part 0) is current device
** Unable to read file boot.scr **
22999552 bytes read in 281 ms (78.1 MiB/s)
Booting from mmc ...
42981 bytes read in 9 ms (4.6 MiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300d7e4
--------------------------------------------------------------------------------------------------------------
How can we resolve it
Regards
Santhosh
解決済! 解決策の投稿を見る。
This issue was solved by adding the MAC address,
setenv ipaddr 192.168.36.126
setenv serverip 192.168.36.10
setenv netmask 255.255.255.0
setenv ethaddr 00:a8:44:1f:1f:10
saveenv
Regards
Santhosh
This issue was solved by adding the MAC address,
setenv ipaddr 192.168.36.126
setenv serverip 192.168.36.10
setenv netmask 255.255.255.0
setenv ethaddr 00:a8:44:1f:1f:10
saveenv
Regards
Santhosh