erofs file system support in android 12 bsp for imx8q-evk board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

erofs file system support in android 12 bsp for imx8q-evk board

ソリューションへジャンプ
273件の閲覧回数
althafahammed
Contributor III

I need to change the file system type to erofs from ext4 in  the boardCommonconfig.mk file

What all changes do i need make to support erofs file system and boot the image properly

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
258件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It is possible but you have to change android completely and build again:

https://source.android.com/docs/core/architecture/kernel/erofs

 

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
259件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It is possible but you have to change android completely and build again:

https://source.android.com/docs/core/architecture/kernel/erofs

 

Regards

0 件の賞賛
返信