erofs file system support in android 12 bsp for imx8q-evk board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

erofs file system support in android 12 bsp for imx8q-evk board

跳至解决方案
279 次查看
althafahammed
Contributor III

I need to change the file system type to erofs from ext4 in  the boardCommonconfig.mk file

What all changes do i need make to support erofs file system and boot the image properly

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
264 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It is possible but you have to change android completely and build again:

https://source.android.com/docs/core/architecture/kernel/erofs

 

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
265 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It is possible but you have to change android completely and build again:

https://source.android.com/docs/core/architecture/kernel/erofs

 

Regards

0 项奖励
回复