erofs file system support in android 12 bsp for imx8q-evk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

erofs file system support in android 12 bsp for imx8q-evk board

Jump to solution
212 Views
althafahammed
Contributor III

I need to change the file system type to erofs from ext4 in  the boardCommonconfig.mk file

What all changes do i need make to support erofs file system and boot the image properly

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
197 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It is possible but you have to change android completely and build again:

https://source.android.com/docs/core/architecture/kernel/erofs

 

Regards

View solution in original post

0 Kudos
Reply
1 Reply
198 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It is possible but you have to change android completely and build again:

https://source.android.com/docs/core/architecture/kernel/erofs

 

Regards

0 Kudos
Reply