encoding to two different H264 resolutions on imx.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

encoding to two different H264 resolutions on imx.6

1,600 Views
liora
Contributor I

Hi All,

I'm trying to setup a gstreamer chain that takes the camera input and encode into two different resolutions:  I get two errors on vpuenc1

negotiation problem

encoder not initialized

Does anyone have a clue about the meaning of this error ?  encoding one copy works fine as well as replacing one of the tee branch with fakesink so this is not an issue of threads etc.....

Thanks

Lior

root@varsomimx6:~#   gst-launch-1.0 imxv4l2src ! videoconvert ! video/x-raw,width=1920,height=1080,format=I420 ! tee name=t  \

>     t. ! queue  ! vpuenc bitrate=2000  ! capsfilter caps="video/x-h264,width=1920,height=1080,framerate=(fraction)30/1" ! matroskamux ! filesink location='/tmp/cap0.mkv' sync=false \

>     t. ! queue  ! videoscale ! video/x-raw,width=640,height=480 !  vpuenc bitrate=1000  ! capsfilter caps="video/x-h264,width=640,height=480,framerate=(fraction)30/1" ! matroskamux ! filesink location='/tmp/cap1.mkv' sync=false

====== IMXV4L2SRC: 4.0.3 build on Aug  4 2015 11:06:57. ======

Setting pipeline to PAUSED ...

[INFO] Product Info: i.MX6Q/D/S

====== VPUENC: 4.0.3 build on Aug  4 2015 11:07:01. ======

  wrapper: 1.0.58 (VPUWRAPPER_ARM_LINUX Build on Aug  4 2015 11:06:35)

  vpulib: 5.4.28

  firmware: 3.1.1.46063

[INFO] Product Info: i.MX6Q/D/S

====== VPUENC: 4.0.3 build on Aug  4 2015 11:07:01. ======

  wrapper: 1.0.58 (VPUWRAPPER_ARM_LINUX Build on Aug  4 2015 11:06:35)

  vpulib: 5.4.28

  firmware: 3.1.1.46063

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

[INFO] ringBufferEnable 0, chromaInterleave 0, mapType 0, linear2TiledEnable 0

ERROR: from element /GstPipeline:pipeline0/GstVpuEnc:vpuenc1: GStreamer error: negotiation problem.

Additional debug info:

/home/variscite/var-som-mx6-yocto-dizzy/build_x11/tmp/work/cortexa9hf-vfp-neon-mx6-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.4.1-r0/gst-plugins-base-1.4.1/gst-libs/gst/video/gstvideoencoder.c(1474): gst_video_encoder_chain (): /GstPipeline:pipeline0/GstVpuEnc:vpuenc1:

encoder not initialized

Execution ended after 0:00:01.048597667

Setting pipeline to PAUSED ...

0 Kudos
Reply
1 Reply

1,199 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please try at first two separate (non parallel) streams with minimal

number gstreamer elements (source -> queue -> sink) – to define

what elements (parameters) are not “compatible”.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply