emwin graphic library with iMXRT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emwin graphic library with iMXRT

698 Views
johnot
Contributor I

Hi ,

 

   Is the emwin graphic library with iMXRT freely available?

Is it possible to use emwin graphic library in imxrt based commercial products free of cost?

 

Best regards,

John OT

0 Kudos
2 Replies

474 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi John OT,

Yes, the emwin graphic library with iMXRT  is freely available. You can use it.

Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

474 Views
johnot
Contributor I

Hi Rita,

 

   Thanks for the quick reply.

 

  Have couple of questions.

  1. We didn't want to use hyper flash, instead we want to use either QSPI or SD card.

  2. Can we use sd card to boot the system and run the emwin gui? Is tools are available to program the SD card from out side and use it in RT board? 

  3. Can we use qspi with emwin gui? Since emwin occupy a bigger amount of memory, is it wise to use QSPI for booting? Is tools are available to program the qspi  with USB/uart  connections with PC?

 

Best regards,

John OT

0 Kudos