my imx6ull connects emmc(MICRON 4GB MTFC4GACAJCN-4MIT
) to usdhc2.
with 8-bit data bus mode :
&usdhc2 {
pinctrl-names = "default", "state_100mhz", "state_200mhz";
pinctrl-0 = <&pinctrl_usdhc2_8bit>;
pinctrl-1 = <&pinctrl_usdhc2_8bit_100mhz>;
pinctrl-2 = <&pinctrl_usdhc2_8bit_200mhz>;
bus-width = <8>;
no-1-8-v;
non-removable;
status = "okay";
};
Write Test CMD: time dd if=/dev/zero of=./500MB bs=1M count=500
Read Test CMD: time dd of=/dev/null if=./500MB bs=1M count=500
Speed: read=20MB/s write=15MB/s (work at MMC_TIMING_MMC_DDR52 )
root@Router:~# cat /sys/kernel/debug/mmc1/ios
clock: 52000000 Hz
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 3 (8 bits)
timing spec: 8 (mmc DDR52)
signal voltage: 0 (3.30 V)
driver type: 0 (driver type B)
if with 4-bit data bus mode :
&usdhc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc2>;
bus-width = <4>;
non-removable;
status = "okay";
};
Speed: read=29MB/s write=15MB/s (work at MMC_TIMING_MMC_DDR52)
I do a test in a 3rd part demo board 100ask_imx6ll (MYIR tech), its speed is only read=30MB/s write=13MB/s.
Also if i replace my imx6ull emmc with SkyHigh's S40FC004C1B1I000 (4GB), the test speed is read=50MB/s write=11MB/s.(also only work at MMC_TIMING_MMC_DDR52 )
What is NXP's EVK board emmc speed test reslut? anyone test for me?
Anyone know why 8-bit mode speed is lower then 4-bit mode?
How to reach a higher MMC HS200 mode ? (RM say imx6ull support HS200 mode)
Solved! Go to Solution.
Yes, For the imx6ull support HS200 mode, for the 8bit support, you need to make imx6ull's emmc controler and emmc flash powered 1.8V, and in the code remove "no-1-8-v;".
For your setting I see you are using the 3.3V, so only 4bit works.
Yes, For the imx6ull support HS200 mode, for the 8bit support, you need to make imx6ull's emmc controler and emmc flash powered 1.8V, and in the code remove "no-1-8-v;".
For your setting I see you are using the 3.3V, so only 4bit works.
Thank you for your professional response,@b45499
You are welcome, wish you have a nice day.
Which version BSP are you using? I will confirm it for you.
the emmc part of our schemetic as below:
our imx6ull's emmc controler and emmc flash are powered 3.3v only, so i add "no-1-8-v;" into usdhc2 node of dts.
Is that right?
&usdhc2 {
pinctrl-names = "default", "state_100mhz", "state_200mhz";
pinctrl-0 = <&pinctrl_usdhc2_8bit>;
pinctrl-1 = <&pinctrl_usdhc2_8bit_100mhz>;
pinctrl-2 = <&pinctrl_usdhc2_8bit_200mhz>;
bus-width = <8>;
no-1-8-v;
non-removable;
status = "okay";
};
if remove "no-1-8-v;" from usdhc2 node of dtsm, our imx6ull probe emmc flash fail.
and i find in linux-imx-5.4.24/drivers/mmc/host/sdhci-esdhc-imx.c
static int
sdhci_esdhc_imx_probe_dt(struct platform_device *pdev,
struct sdhci_host *host,
struct pltfm_imx_data *imx_data)
{
...
if (of_find_property(np, "no-1-8-v", NULL))
host->quirks2 |= SDHCI_QUIRK2_NO_1_8_V;
...
}
and i find in linux-imx-5.4.24/drivers/mmc/host/sdhci.c
if (host->quirks2 & SDHCI_QUIRK2_NO_1_8_V) {
host->caps1 &= ~(SDHCI_SUPPORT_SDR104 | SDHCI_SUPPORT_SDR50 |
SDHCI_SUPPORT_DDR50);
/*
* The SDHCI controller in a SoC might support HS200/HS400
* (indicated using mmc-hs200-1_8v/mmc-hs400-1_8v dt property),
* but if the board is modeled such that the IO lines are not
* connected to 1.8v then HS200/HS400 cannot be supported.
* Disable HS200/HS400 if the board does not have 1.8v connected
* to the IO lines. (Applicable for other modes in 1.8v)
*/
mmc->caps2 &= ~(MMC_CAP2_HSX00_1_8V | MMC_CAP2_HS400_ES);
mmc->caps &= ~(MMC_CAP_1_8V_DDR | MMC_CAP_UHS);
}
those two infos make we confuse?
how to let our imx6's emmc reach a higher speed?
we use the kernel pulled from NXP's https://source.codeaurora.org/external/imx/linux-imx branch imx_5.4.24_2.1.0 recently.