I am using i.MX RT1064. I have taken emWin from what has been included in SDK_2.x_EVK-MIMXRT1064 version 2.8.0. When I am using FreeRTOS with multiple tasks (one taking care of touch, one emwin, one other sensors) with this environment, after calling GUIExec() (which returns just fine), it seems that another task does not get runtime anymore (it is waiting in xTaskNotifyWait). Otherwise I can see in the screen what I am supposed to, and changing emWin views works fine.
One thing I was wondering, is that the GUI_X_ExecIdle is never called, although according to emwin specification GUI_X_ExecIdle is "Called when there are no longer any messages which require processing. In this case the GUI is up to date."
Does anyone have ideas on this issue? Should FreeRTOS and emWin work together in i.MX RT1064?
解決済! 解決策の投稿を見る。
Hi!
I was able to solve this issue, it was due to too small stack size.
Br, Gamka
Hi Gamka:
Normally in a multiple tasks environment, the real time critical tasks will have the highest priorities. and the tasks which used for the user interface calling emWin functions, these tasks typically have low priorities in the system.
I would suggest you adjust the priorities of your system first.
Regards
Daniel