Hello everyone!
I have a problem with elftosb2 as it constructs .sb image with instructions to load virtual addresses instead of physical.
I have elf binary for which "readelf -e" reports:
...
Section Headers:
[Nr] Name Type Addr Off Size ES Flg Lk Inf Al
[ 0] NULL 00000000 000000 000000 00 0 0 0
[ 1] .start PROGBITS 40000000 008000 0000ec 00 AX 0 0 4
[ 2] .text PROGBITS c00000ec 0080ec 14f5c4 00 AX 0 0 128
...cut...
Program Headers:
Type Offset VirtAddr PhysAddr FileSiz MemSiz Flg Align
LOAD 0x008000 0x40000000 0x40000000 0x000ec 0x000ec R E 0x8000
LOAD 0x0080ec 0xc00000ec 0x400000ec 0x14f6c4 0x14f6c4 R E 0x8000
LOAD 0x158000 0xc0150000 0x40150000 0xcb040 0xdacf4 RW 0x8000
I'd like to SB image to load code to PhysAddresses, instead of Virt.
Snipplet from the .bd:
// Load kernel to DRAM. | |
load kernel; | |
jump kernel; |
And output from the elftosb:
$ nbelftosb -V -c bootimx23.bd -z -o bootimx23.sb
Boot Section 0x00000000:
LOAD | adr=0x00000000 | len=0x00001008 | crc=0xa9094f19 | flg=0x00000000
LOAD | adr=0x00001008 | len=0x00000064 | crc=0xf3c1ca49 | flg=0x00000000
FILL | adr=0x0000106c | len=0x0000000c | ptn=0x00000000
CALL | adr=0x000001a8 | arg=0x00000000 | flg=0x00000000
LOAD | adr=0x40000000 | len=0x000000ec | crc=0x5e621393 | flg=0x00000000
LOAD | adr=0xc00000ec | len=0x0014f5c4 | crc=0x42e999c0 | flg=0x00000000
LOAD | adr=0xc014f6b0 | len=0x0000003c | crc=0xa8b3e4a6 | flg=0x00000000
LOAD | adr=0xc014f6ec | len=0x0000000c | crc=0x7a350852 | flg=0x00000000
LOAD | adr=0xc014f6f8 | len=0x0000004c | crc=0xa2ae784a | flg=0x00000000
LOAD | adr=0xc014f744 | len=0x00000004 | crc=0x02b0032f | flg=0x00000000
LOAD | adr=0xc014f748 | len=0x00000038 | crc=0x7186ee9b | flg=0x00000000
LOAD | adr=0xc014f780 | len=0x00000010 | crc=0xa5cac6ee | flg=0x00000000
LOAD | adr=0xc014f790 | len=0x00000020 | crc=0x29c7ba54 | flg=0x00000000
LOAD | adr=0xc0150000 | len=0x000cb040 | crc=0x8446f74b | flg=0x00000000
FILL | adr=0xc021b040 | len=0x0000fcb4 | ptn=0x00000000
JUMP | adr=0x40000000 | arg=0x00000000 | flg=0x00000000
As you can see, elftosb2 load to Virtual. I'd like to have it to load using ELF binary's physcall address to do the loads.
Is it possible? Is it known issue? I've read the fine manual and I didn't find anything which relates this problem.
Best regards
Petri Laakso
解決済! 解決策の投稿を見る。
I solved this problem by copying elf binary's data using objcopy and loading resulting raw. Something like:
sources {
# elf(3) binary.
boot_prep="./boot";
# objcopy(1) generated .bin
kernel="./kernel.bin";
}
section (0) {
// Initialize power, clocks and DRAM.
load boot_prep;
call boot_prep;
// Load kernel to DRAM.
load kernel > 0x40000000;
jump 0x40000000;
}
what BSP are you using? what board are you using?
i.MX23 OLinuXino and vanilla elftosb compiled from the source.
So, the question is, am I able to instruct elftosb to use ELF binary's physical addresses, instead of virtual?
I'd like to load all sections to starting from 0x40000000, as it is DRAM address space.
There is nothing physically or rather, virtually mapped to 0xc0000000 :-(
I solved this problem by copying elf binary's data using objcopy and loading resulting raw. Something like:
sources {
# elf(3) binary.
boot_prep="./boot";
# objcopy(1) generated .bin
kernel="./kernel.bin";
}
section (0) {
// Initialize power, clocks and DRAM.
load boot_prep;
call boot_prep;
// Load kernel to DRAM.
load kernel > 0x40000000;
jump 0x40000000;
}