ehci driver "port test control"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ehci driver "port test control"

1,993件の閲覧回数
satheshkumarman
Contributor II

Hello,

I'm using the linux v 3.13.0 / IMX6. We need to validate USB test modes as specified in USB 2.0

I have understand that, the ehci-hub driver is limited to support test modes from 01 (J_STATE)  to 05 (FORCE_ENABLE_HS).

Since the test modes 06 (FORCE_ENABLE_FS) and 07 (FORCE_ENABLE_LS) also specified in USB 2.0, why these test modes are limited from ehci-hub driver?

Untitled.png

I can update the driver to remove this limitation, but what would be reason these tests are limited in the driver?

Thanks in advance.

Best Regards

Sathesh

ラベル(7)
0 件の賞賛
返信
4 返答(返信)

1,806件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Hi Satesh,

Please post this question to the linux-usb@vger.kernel.org mailing list.

Regards,

Fabio Estevam

0 件の賞賛
返信

1,806件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

our official BSP is no ver 3.13.0

0 件の賞賛
返信

1,806件の閲覧回数
satheshkumarman
Contributor II

Hello Jimmy,

Thanks for your reply.

yes. I'm using the same BSP version.

Please advice.

Thanks.

Sathesh

0 件の賞賛
返信

1,806件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I mean we don't have ver 3.13.0.

We have 3.10.53 and 3.10.17.

You can download the BSP from here:

i.MX 6 Series Software and Development Tool R|Freescale

0 件の賞賛
返信