Hi,
I build weston-1.5.0 with this tutorial :
Building Wayland-Weston for i.MX6
weston-1.5.0 was downloaded from : Wayland
gpu module :gpu-viv-bin-mx6q-3.10.17-1.0.0
board : mcimx6q-sdb
kernel : yocto 3.10.17
After install, weston could be launched. In weston terminal, I always get a error when launching "weston-simple-egl".
weston-simple-egl: clients/simple-egl.c:151: init_egl:Assertion "ret==1" failed.
Aborted (core dumped)
I checked the source code and found out it was function "eglInitialize()" failed.
I use the same way to build weston-1.4.0,and "weston-simple-egl" could be launched successfully.
Does this gpu module support weston-1.5.0 ? Could anyone help me?
Thanks
I can run Weston 1.5 and 1.6 under i.mx6 with kernel 3.10.17.1.0.0.1-ga. The rootfs is build with Yocto.
The weston-simple-egl also works fine.
It seems like you neet to patch weston to make it work.
for more info, please see: meta-freesacle-arm 's recipes