eglImage vs glTexDirectVIV

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eglImage vs glTexDirectVIV

1,513 Views
volki
Contributor III

I'm currently try to port our cross platform framework to different architectures. So far every platform supported EGLImage extension by using EGL_NATIVE_PIXMAP_KHR. I found some examples for the iMX53 to get it running with EGL_NEW_IMAGE_FSL but this seems to be not supported by the iMX6, is it? Also I would prefer to have the official khronos extension EGL_NATIVE_PIXMAP_KHR instead of a proprietary FSL one.

The things that bugs me most is the lack of official documentation. Are there also some hints what's the best practice regarding streaming texture uploads? I know there are glTexDirectVIV methods available (although there is also a lack of documentation especially regarding thread safeness) but since this is again a proprietary extension, I wonder if it isn't possible to use an EGLImage with the same performance.  But I couldn't even found some information about possible image formats for an EGLImage, in case the iMX6 supports this extension at all.

Labels (1)
Tags (3)
0 Replies