Hi,
I am posting the query again, similar query has been posted long back by myself. please find below the previous post details.
https://community.nxp.com/t5/i-MX-Processors/iMX8MM-ECSPI-DMA-Issue/td-p/1166322
we are now making a custom board with i.mx8mm but the linux kernel will be 4.14
so i would like to request is there any test code to perform the ecspi dma mode test on i.mx8mm evk
and
also please let me know the exact linux kernel version in which ecspi dma mode is perfectly working.
I will try to port it to 4,14 version.
due to the current pandemic situation, i am unable to visit the hw lab for debugging.
please provide your suggestions
Thank you, Sreedhar
Solved! Go to Solution.
Hi
New versions all can support DMA mode
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/spi/spi-imx.c?h=imx_5.4.70_2.3.0
Main function in spi-imx.c is spi_imx_dma_transfer
I didn't find spi dma test
BR
Zhiming
Hi
New versions all can support DMA mode
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/spi/spi-imx.c?h=imx_5.4.70_2.3.0
Main function in spi-imx.c is spi_imx_dma_transfer
I didn't find spi dma test
BR
Zhiming
iMX8MM ECSPI DMA Issue - NXP Community
I am working with i.MX8MM EVK and 4.19.35.1.1.0 Yocto distribution.
We have interfaced a slave to ECSPI2 pins exposed on J1003 of i.MX8MM EVK.
ECSPI2 is configured as Master, CPOL = CPHA = 0, Bits Per Word = 8
The link says slave mode.
It is silicon errata ERR009535, that is why the ecspi driver slave is PIO mode.
NXP Semiconductors IMX8MM_0N87W
Mask Set Errata Rev. 1, 09/2021
Mask Set Errata for Mask 0N87W
IMX8MM_0N87W.pdf
linux-imx/drivers/spi/spi-imx.c”, function “spi_imx_can_dma()”.
static bool spi_imx_can_dma(struct spi_master *master, struct spi_device *spi,
struct spi_transfer *transfer)
{
struct spi_imx_data *spi_imx = spi_master_get_devdata(master);
if (!use_dma || master->fallback)
return false;
if (!master->dma_rx)
return false;
if (spi_imx->slave_mode)
return false;
if (transfer->len < spi_imx->devtype_data->fifo_size)
return false;
spi_imx->dynamic_burst = 0;
return true;
}
Hi,
May I ask a question, is this new version valid for ECSPI in master mode to support DMA mode? Can DMA mode be supported while ECSPI works in slave mode? thanks @Qmiller
B.R.
Guangyu
Guangyu,
Because of the silicon bug the ecspi could not use dma under slave mode.
You are very professional.
Thank you Zhiming !!