eMMC on iMX6 high latency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC on iMX6 high latency

701 Views
EinarMar
Contributor IV

I have a MTFC8GLDDQ-4M eMMC NAND flash from Micron and a custom made board with iMX6Q on it.

My system setup is as following:

kernel: 3.10.17 (RT patched) minor boot customization for our board

uboot: 2014

rootfs: in-house (hard compiled) 

toolchain: Linaro gcc 4.7.2

The system is working fine except the high latency in disk I/O, running the command sync can sometime take 4-5 seconds.

I have tried to backport the mmc driver from kernel 4.2 without any success.

I have also tried various RT settings for the mmc/jbd kernel threads and played around with the dirty_ratio and other settings in /proc/sys/vm without any major difference.

Before I go and dive into the driver I liked to ask if this is a known problem or not ?

kind regards

Einar

Labels (2)
0 Kudos
2 Replies

434 Views
art
NXP Employee
NXP Employee

No, this is not a known problem.


Have a great day,
Artur

0 Kudos

434 Views
EinarMar
Contributor IV

HI Artur and thank you for your response.

regards

Einar

0 Kudos