eMMC not visible in u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eMMC not visible in u-boot

3,642 次查看
antonioramos
Contributor I

Please see the listing below.

 

=>  mmc list

FSL_SDHC: 0 (SD)

FSL_SDHC: 1

=> ls mmc 1:1

  1000000   random_data1

 

1 file(s), 0 dir(s)

 

=>  mmc list

FSL_SDHC: 0 (SD)

FSL_SDHC: 1 (eMMC)

 

Why is it that “mmc list” shows the eMMC after listing the directory but not before? Is this a bug or a feature?

 

I am using a board designed by ourselves based on the iMX6UL EVK. I am using my own image created with Buildroot using the Linux kernel and U-Boot from the 4.9 release by NXP. We have a MicroSD cage from which I am currently booting connected to port 1 and connected to port 2 we have Kingston EMMC04G-M627-Y02U eMMC (eMMC v5.1 compatible with v4.5). Once Linux boots I can (on eMMC) create partitions, format them and copy data, so everything seems fine in Linux so far.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

2,876 次查看
igorpadykov
NXP Employee
NXP Employee

Hi antonioramos 

one can try with nxp uboot imx_v2017.03 :

uboot-imx - i.MX U-Boot 

and use yocto for build, Yocto Guide guidelines from

Documentation package

https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS 

Also may be recommended to post issue on uboot mail list

U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,876 次查看
antonioramos
Contributor I

Hi Igor,

That is the exact u-boot version that I am using, I downloaded it from the NXP git repo. And I am using the defconfig from the evk.

U-Boot 2017.03 (Feb 23 2018 - 17:02:39 +0000)

CPU:   Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 61C
Reset cause: WDOG
Model: Freescale i.MX6 UltraLite 14x14 EVK Board
Board: MX6UL 14x14 EVK
DRAM:  512 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1

Thanks, I will try something else.

Antonio

0 项奖励
回复