eMMC not booting in imx6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC not booting in imx6UL

Jump to solution
2,966 Views
obulesu_veggidi
Contributor II

Hi,

With Our custom imx6UL board I am able to boot from SD card, and I flashed/copied the images to emmc(mmcblk1). But I am not able to boot the device from eMMC. Device is loading with u-boot and throwing following error.

U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+ga57b13b (Sep 23 2020 - 18:38:35 +0530)

CPU: Freescale i.MX6UL rev1.2 at 396 MHz
Reset cause: POR
Board: MX6UL 14X14 DDR3 ARM2
I2C: ready
DRAM: 1 GiB
force_idle_bus: sda=0 scl=1 sda.gp=0x3 scl.gp=0x2
force_idle_bus: failed to clear bus, sda=0 scl=1
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Card did not respond to voltage select!
*** Warning - MMC init failed, using default environment

Display: MCIMX28LCD (800x480)
Video: 800x480x24
In: serial
Out: serial
Err: serial
Card did not respond to voltage select!
Net: FEC1 MXC: board_eth_init:failed
No ethernet found.
Normal Boot
Hit any key to stop autoboot: 0
Card did not respond to voltage select! 
Card did not respond to voltage select!
Card did not respond to voltage select!
Booting from net ...
No ethernet found.
No ethernet found.
Bad Linux ARM zImage magic!
=>

 

Pls help me to resolve the above error.

Thanks in advance.

0 Kudos
Reply
1 Solution
2,953 Views
igorpadykov
NXP Employee
NXP Employee

Hi obulesu_veggidi

 

for "Card did not respond to voltage select!" error one can look hints on

https://community.nxp.com/t5/i-MX-Processors/iMX6q-Sabre-lite-board-Card-did-not-respond-to-voltage-...

also one can try "mx6ul_14x14_evk" instead "MX6UL 14X14 DDR3 ARM2"

https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6ul_14x14_evk?h=nxp/imx_...

 

Best regards
igor

 

View solution in original post

2 Replies
2,954 Views
igorpadykov
NXP Employee
NXP Employee

Hi obulesu_veggidi

 

for "Card did not respond to voltage select!" error one can look hints on

https://community.nxp.com/t5/i-MX-Processors/iMX6q-Sabre-lite-board-Card-did-not-respond-to-voltage-...

also one can try "mx6ul_14x14_evk" instead "MX6UL 14X14 DDR3 ARM2"

https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx6ul_14x14_evk?h=nxp/imx_...

 

Best regards
igor

 

2,946 Views
obulesu_veggidi
Contributor II

Hi Igor,

 

Thanks for your reply. my issue is resolved. Now I want to flash the images to emmc using usb port and i want to program some fuses for secure boot in production environment for our custom board. how this can happen in a single click. Pls suggest me a solution.

Thanks in advance.

0 Kudos
Reply