eMMC is used in IMX8M Plus app

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC is used in IMX8M Plus app

Jump to solution
2,306 Views
www1519
Contributor III

Hi! NXP Engineer

In my design,IMX8M Plus + eMMC(SDINBDG4-8G) is used.

the schematic is refer to NXP development kit.

eMMC’s PS is from PCA9450C.

But, when boot form eMMC,the error is below.

Only one  board (others is ok)has error as shown in the following capture.

Even if SoC and eMMC exchange with new parts, the phenomenon still does not disappear.

Pls help to resolute this. Thanks.

 

www1519_0-1682333857769.png

 

www1519_0-1682333562925.png

www1519_1-1682333908348.png

 

0 Kudos
Reply
1 Solution
2,085 Views
www1519
Contributor III

Hi Chavira @Chavira 

I'm very sorry for the late reply.

the above problem has been solved.

Thank you for support.

Best regard!

View solution in original post

9 Replies
2,272 Views
www1519
Contributor III

Hi! Chavira @Chavira 

Thank you for  your reply.

Yes, only one board.

In manufacture,check it using an X-Ray,but  the connection is normal.

so, I don‘t know how to reserach it.

thanks best regard.

 

 

0 Kudos
Reply
2,284 Views
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

Do you only have one board with the failure?

I recommend checking if the Processor is soldered correctly, please check the connections using an X-ray.

0 Kudos
Reply
2,272 Views
www1519
Contributor III

Hi! Chavira @Chavira 

Thank you for  your reply.

Yes, only one board.

In manufacture,check it using an X-Ray,but  the connection is normal.

so, I don‘t know how to reserach it.

0 Kudos
Reply
2,260 Views
Chavira
NXP TechSupport
NXP TechSupport

In this case, I recommend checking all the voltages, if all the voltages are good, please check all the resistors of the MMC, and for the last task, please check all the signals with an oscilloscope or logic analyzer.
Please compare each signal with a functional board.

0 Kudos
Reply
2,247 Views
www1519
Contributor III

Hi! Mr. Chavira @Chavira 

Thank you for reply.

1. I have checked all singals with an oscilloscope, but Data Strobe singal always is low level.

    I think that the other sigals are coincident. It is strange.

2. 4/21 I have checked PS, all are right.

    Just I check PS again, and P1.8D from PCA9450C has became 3.3V.

    PCA9450C is damaged?

www1519_0-1682508897937.png

 

best regards.

 

 

 

 

Tags (1)
0 Kudos
Reply
2,240 Views
Chavira
NXP TechSupport
NXP TechSupport

Check the signal SD_VSEL of the PMIC (pin 29)

Chavira_0-1682523943388.png

If the SD_VSEL is ok, you can reconfigure the PMIC configuring the Register "BUCK5CTRL" Please check the details on page 43 of the datasheet.

Power management IC for i.MX 8M application processor family (nxp.com)

 

0 Kudos
Reply
2,231 Views
www1519
Contributor III

Hi! Chavira @Chavira

Thanks for reply.

As datasheet, Buck5(P1.8V) is not related to  SD_VSEL.

Load Switch output voltage is decided by SD_VSEL.

I think that the PCA9540C may be demaged.

(this board firmware is the same as the other PCB board )

best regards.

 

 

0 Kudos
Reply
2,220 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @www1519 

I think that PMIC only needs a reconfiguration.

If you think that PMIC is damaged, please replace it with a new one and contact your sales to obtain a warranty.

Best Regards.

 

0 Kudos
Reply
2,086 Views
www1519
Contributor III

Hi Chavira @Chavira 

I'm very sorry for the late reply.

the above problem has been solved.

Thank you for support.

Best regard!