eMMC connection with i.MX8M Mini Quad Core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMC connection with i.MX8M Mini Quad Core

2,428件の閲覧回数
nija_mankodi
Contributor II

Hi,

We are using i.MX8M Mini Quad core processor in our device. We have connected eMMC 8GB/16GB on NAND as per attached image. eMMC part# is MTFC8GAKAJCN-1M WT (8GB)/MTFC16GAPALBH-IT  (16GB).

We have connected our WiFi module on SD1 port and SD2 port is used as GPIO.

Please confirm whether we can connect eMMC on NAND port or not as shown in attached image.

Please respond on this ASAP. eMMC datasheet is also attached.

ラベル(1)
0 件の賞賛
返信
1 返信

2,348件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Yes it shouldn't have a problem, please refer to i.MX 8MM datasheet section 4.2 Boot device interface allocation:

 pastedImage_2.png

 

Also, for a new design you can always take a look to our EVK schematic and layout for reference:

https://www.nxp.com/webapp/Download?colCode=8MMINILPD4-EVK-DESIGNFILES

 

Hope this helps,

Regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信