eMMC card struck error in imx6 4.1.15 krenel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC card struck error in imx6 4.1.15 krenel

1,261 Views
shabeerbadarudh
Contributor IV

Hi,

We have ported i.MX6 linux kernel 4.1.15 to our custom board and seeing an error/warning message related to eMMC memory while boot time .

mmc0: Card stuck in programming state! __mmc_switch
blk_update_request: I/O error, dev mmcblk0boot0, sector 32640

Initially these error logs are getting frequently, then based on the link https://bugs.launchpad.net/ubuntu/+source/systemd/+bug/1333140
we have modified the udev rule. Then the frequency of occurring error is reduced, but still we are getting the error message. Is these log indicate any serious issue or can we ignore it? Anyone could help us to resolve the issue?

System Details:

Processor - i.MX6 Solo 

eMMC - Micron

kernel - 4.1.15

Thanks

Shabeer

0 Kudos
2 Replies

698 Views
shabeerbadarudh
Contributor IV

Hi igorpadykov,

Thanks for the response, we will test above mentioned patch!

Thanks,

Shabeer 

0 Kudos

698 Views
igorpadykov
NXP Employee
NXP Employee

HI Shabeer

one can try patch on

[meta-freescale] [meta-fsl-ppc][PATCH 2/4] udev[-extraconf]: skip mmc rpmb partitions 

or post this on mainline linux mail list, as this is common linux issue.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos