eMMC Booting fails in imx6q sabresdp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC Booting fails in imx6q sabresdp

619 Views
kalaranjani086
Contributor I

Hello All,

            I am currently working under eMMC boot in iMX6 SABRE-SDP, So i followed the Android Frequently Asked Questions guide for boot using fastboot q tool.

The method which i made is that,

i have entered in the u-boot as,

U-Boot > fastboot q

fastboot is in init......flash target is MMC:1

USB Mini b cable Connected!

Then i placed the eMMC images in image folder,

Here i can able to flash the images to the corresponding devices.I changed to the SW6 switch to 11010110 .But when i used to enter fastboot reboot, it shows me it is getting resetted, even after along time also there is no changes in the output screen.

Note: The images i used is of android_jb4.2.2_1.0.0-ga_image_6qsabresd, eMMC->system.img,recovery.img,boot.img,u-boot(no padding) .

But still there is no changes in the output screen.

Labels (1)
0 Kudos
0 Replies