eMMC 5.0 support in i.MX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMC 5.0 support in i.MX6Q

ソリューションへジャンプ
1,839件の閲覧回数
vishakh
Contributor III

Hi,

We are developing a custom board based on i.MX6Q. Here we need to connect eMMC 5.0(with data strobe signal NC).

Based on the discussion in https://community.freescale.com/thread/325001#comment-409823, it is possible to connect eMMC 5.0 to i.MX6Q(with driver modification).

Can we follow the same procedure(by changing the check value of card->ext_csd.rev) in linux 3.0.35?

Will it be possible to boot from eMMC, without any concerns on flashing eMMC from MFG tool?

Thanks and Regards,

Vishakh

ラベル(1)
0 件の賞賛
返信
1 解決策
1,306件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Vishakh,

Yes, you just need to modify the value of card->ext_csd.rev as you see in that thread, The default emmc supported is eMMC 4.4 in linux 3.0.35. after you change it then the eMMC 5.0 can work as an eMMC 4.4.  And there is no concerns on flashing eMMC from MFG tool. :smileyhappy:
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,307件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Vishakh,

Yes, you just need to modify the value of card->ext_csd.rev as you see in that thread, The default emmc supported is eMMC 4.4 in linux 3.0.35. after you change it then the eMMC 5.0 can work as an eMMC 4.4.  And there is no concerns on flashing eMMC from MFG tool. :smileyhappy:
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信