eIQ Tensorflow-lite c++ on NPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eIQ Tensorflow-lite c++ on NPU

Jump to solution
7,777 Views
rbanks
Contributor III

I am developing on an 8Mplus board and have had some issues with TensorFlow-Lite in c++.

I have my own TensorFlow-Lite model and want to utilize it in my c++ application. I have found that the eIQ software installed with Yocto doesn't come with a static library for TensorFlow-lite.

None of the guides describe how to build a Yocto image with a static library for TensorFlow-Lite. I've had to piece parts of several guides in order to even get the TensorFlow-Lite header files.

Is there a known step by step method to build a Yocto image of the imx 8Mplus dev board with a Static Library or some other method of linking the c++ TensorFlow-Lite binaries while allowing TensorFlow-Lite to utilize the NPU?

 

0 Kudos
Reply
1 Solution
7,605 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

After some builds and some search, I found this:

https://stackoverflow.com/questions/55125977/how-to-build-tensorflow-lite-as-a-static-library-and-li...

 

I can also see this:

yocto/imx-5.4.47-2.2.0/bld-xwayland$ find -name libtensorflow*a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/git/tensorflow/lite/tools/make/gen/linux_aarch64/lib/libtensorflow-lite.a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/sysroot-destdir/usr/lib/libtensorflow-lite.a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/image/usr/lib/libtensorflow-lite.a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/package/usr/lib/libtensorflow-lite.a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/packages-split/tensorflow-lite-staticdev/usr/lib/libtensorflow-lite.a
./tmp/sysroots-components/aarch64/tensorflow-lite/usr/lib/libtensorflow-lite.a

 

so, the libtensorflow-lite.a is being installed when you install the tensorflow-lite-staticdev lib. However from the original message "I have my own TensorFlow-Lite model"

It might be that some adjustments should be done in the CMake environment so that all the static libs needed are being built/created.

Could you, please, share exactly which is the error log?

 

Regards

 

View solution in original post

0 Kudos
Reply
15 Replies
7,766 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello rbanks.

I found this info on Yocto User Guide, could you please try adding the following line to your local.conf?
 
TOOLCHAIN_TARGET_TASK_append += " tensorflow-lite-staticdev tensorflow-lite-dev"
 
Please, let me know if this works or not for you
 
Regards

 

0 Kudos
Reply
7,754 Views
rbanks
Contributor III

Hi Bio_TICFSL,

My local.conf file looks as follow:

MACHINE ??= 'imx8mpevk'
DISTRO ?= 'fsl-imx-xwayland'
PACKAGE_CLASSES ?= 'package_rpm'
EXTRA_IMAGE_FEATURES ?= "dev-pkgs debug-tweaks tools-debug tools-sdk ssh-server-openssh"
IMAGE_INSTALL_append = "opencv git wget cmake"

TOOLCHAIN_TARGET_TASK += "tensorflow-lite-dev tensorflow-lite-staticdev"

USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS ??= "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
ABORT,${TMPDIR},100M,1K \
ABORT,${DL_DIR},100M,1K \
ABORT,${SSTATE_DIR},100M,1K \
ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-system-native = " sdl"
CONF_VERSION = "1"

DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"

# Switch to Debian packaging and include package-management in the image
PACKAGE_CLASSES = "package_deb"
EXTRA_IMAGE_FEATURES += "package-management"


The line TOOLCHAIN_TARGET_TASK_append += " tensorflow-lite-staticdev tensorflow-lite-dev" only adds header files. The static library is  no where to be found or perhaps not named as expected.

0 Kudos
Reply
7,744 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

I understand you have a package that you are building against the tensorflow-lite, right?

Are you using DEPENDS += "tensorflow-lite" inside the recipe of your package?

Regards

 

0 Kudos
Reply
7,722 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

It seems that the TensorFlow libraries are in the Yocto project but it is not integrated into the rootfs.

Could you please check in your build project at this path?

bld-xwayland/tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/git/tensorflow/lite/tools/make/gen/linux_aarch64/lib/libtensorflow-lite.a

Please, let me know!

 

0 Kudos
Reply
7,708 Views
rbanks
Contributor III

So what does that mean? After I run bitbake on the build directory the resulting image is missing libtensorflow-lite.a. Are you implying that I can copy that static library to the image?

Is that static library compiled to use the NPU?

0 Kudos
Reply
7,714 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

libtensorflow-lite.a does exist in the build directory at that location.

 

0 Kudos
Reply
7,720 Views
rbanks
Contributor III

libtensorflow-lite.a does exist in the build directory at that location.

0 Kudos
Reply
7,696 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

That basically means that *.a files are not intended to be installed on a image rootfs, as they are development files only.

 

The *.a files should be part of the -dev packages, or installed on a SDK image (toolchain)

 

That's why it's important to understand how you are integrating the package recipe, or if they are working on a native build system, or developing the package only using the SDK (toolchain)

 

Could you, please confirm which tensorflow-lite recipe are you using on your tests?

Would be this one?

https://source.codeaurora.org/external/imx/meta-imx/tree/meta-ml/recipes-libraries/tensorflow-lite/t...

 

I want to test locally to make sure the recipe does not have a bug on that installation. Could you, please, confirm that?

 

Regards

 

0 Kudos
Reply
7,651 Views
rbanks
Contributor III

Were you able to verify that the recipe doesn't have a bug?

0 Kudos
Reply
7,644 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, it don´t have a bug.

 

0 Kudos
Reply
7,638 Views
rbanks
Contributor III

So when you build the recipe and then flash an SD card, the libtensorflow-lite.a file exists in the image?

 

If that is true, can you provide the step by step solution that you used to get there? Nothing I try has given me the desired results.

0 Kudos
Reply
7,676 Views
rbanks
Contributor III

I think I understand what you are getting at.

On my native build machine at yocto_build/source/meta-imx/meta-ml/recipes-libraries/tensorflow-lite exists the file tensorflow-lite_2.2.0.bb. I did a file compare to the one you linked and they are identical.

I am also using Ubuntu 18.04 but I would hope that that isn't the problem as I don't want to have to spend the day or so rebuilding my environment in Ubuntu 16.04.

Thanks for your help on this.

0 Kudos
Reply
7,738 Views
rbanks
Contributor III

I have my own c++ code that utilizes the TensorFlow-Lite static library. I need to be able to run make on my code which requires the tensorflow-lite static library. I'm rather new to Yocto. Where would I add DEPENDS += "tensorflow-lite"?

0 Kudos
Reply
7,606 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

After some builds and some search, I found this:

https://stackoverflow.com/questions/55125977/how-to-build-tensorflow-lite-as-a-static-library-and-li...

 

I can also see this:

yocto/imx-5.4.47-2.2.0/bld-xwayland$ find -name libtensorflow*a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/git/tensorflow/lite/tools/make/gen/linux_aarch64/lib/libtensorflow-lite.a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/sysroot-destdir/usr/lib/libtensorflow-lite.a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/image/usr/lib/libtensorflow-lite.a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/package/usr/lib/libtensorflow-lite.a
./tmp/work/aarch64-poky-linux/tensorflow-lite/2.2.0-r0/packages-split/tensorflow-lite-staticdev/usr/lib/libtensorflow-lite.a
./tmp/sysroots-components/aarch64/tensorflow-lite/usr/lib/libtensorflow-lite.a

 

so, the libtensorflow-lite.a is being installed when you install the tensorflow-lite-staticdev lib. However from the original message "I have my own TensorFlow-Lite model"

It might be that some adjustments should be done in the CMake environment so that all the static libs needed are being built/created.

Could you, please, share exactly which is the error log?

 

Regards

 

0 Kudos
Reply
7,396 Views
rbanks
Contributor III

Sorry it took so long to get back to this. There seems to be some discrepancy between what you mean and what I mean. I was trying to get the static library on the end device. You are talking about building my app on a host computer. Either way is fine as long as the static library is compiled to take advantage of the end device hardware.

0 Kudos
Reply