eGalax calibration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eGalax calibration

1,898 次查看
dorel
Contributor I

Hi ,

i have imx6 base board(Udoo quad) with android 4.3

I have a problem with  resistive egalax touchscreen.

It's fliped up side down / swap y .

Question is how to calibrate the touchscreen? the program witch is installed on android for calibration, not recognize my touchscreen.

Where i can find the file witch have the settings for touchscreen?

Thank you.

Sorry for my English.

标签 (2)
0 项奖励
回复
1 回复

1,232 次查看
dorel
Contributor I

Nobody? :smileysad:

Is this so hard for you guys?

Maybe this can help a litlle.

root@udoo:/ # su -- getevent -lp /dev/input/event0

add device 1: /dev/input/event0

  name:     "eGalax Inc. USB TouchController"

  events:

    KEY (0001): BTN_TOUCH           

    ABS (0003): ABS_X                 : value 1322, min 0, max 2047, fuzz 0, flat 0, resolution 0

                         ABS_Y                 : value 1119, min 0, max 2047, fuzz 0, flat 0, resolution 0

  input props:

    <none>

root@udoo:/ #

0 项奖励
回复