eDMA LPSPI FreeRTOS RT1160

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eDMA LPSPI FreeRTOS RT1160

ソリューションへジャンプ
1,791件の閲覧回数
neo2
Contributor III

Hi,

I have RT1160, is there a eDMA LPSPI driver for FreeRTOS?

I'm looking at creating one in a similar structure as I2C.

Regards

0 件の賞賛
返信
1 解決策
1,782件の閲覧回数
neo2
Contributor III

Actually I found the best way is to base software the evkmimxrt1160_lpspi_edma_b2b_transfer_master_cm7

I can put the code in it's own task.

I've noted the concept is slightly different from, for example the I2C FreeRTOS example

元の投稿で解決策を見る

1 返信
1,783件の閲覧回数
neo2
Contributor III

Actually I found the best way is to base software the evkmimxrt1160_lpspi_edma_b2b_transfer_master_cm7

I can put the code in it's own task.

I've noted the concept is slightly different from, for example the I2C FreeRTOS example