Hello,
In errata sheet of imx6ul, ERR009606 eCSPI: In master mode, burst lengths of 32n + 1 will transmit
incorrect data, this issue is mentioned. As I understood, there is problem in ecSPI when burst lenght is configured as 32n+ 1 ( where n= 0,1,2,3 ...).
We are using the SPI in master mode with max14830 as slave, so I am looking to check this issue with reproduce. How i can reproduce this issue ?
In workaround it mentioned that, dont use the burst lenght of 32n+ 1.
In the linux driver, where exactly need to configure the burst lenght ?
Regards,
Surendra
The Linux driver only supports the eCSPI transfer lengths of multiple of 8 bits (1 byte), so, no issue will occur there.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------