e-CAM130_iMX8M - 13MP Auto Focus Camera Board for i.MX8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

e-CAM130_iMX8M - 13MP Auto Focus Camera Board for i.MX8

2,031 次查看
dharmalingam
Contributor IV

e-CAM130_iMX8 is a 13MP 4-lane MIPI CSI-2 autofocus camera board for Variscite's DART-MX8M Evaluation kit (VAR-DVK-DT8M). This iMX8 camera can be directly connected to the serial camera connector (J11) of the VAR-DT8M CustomBoard. e-CAM130_iMX8 comes with an high-performance Image Signal Processor (ISP) that performs all the Auto functions (autofocus, auto white balance, auto exposure control). e-CAM130_iMX8 can stream Full HD 1080p@60fps and also supports 4K@15fps.

13mp_autofocus_camera_kit_content_zoom.jpg13mp_autofocus_cameraboard_zoom.jpg

Pic 1: 13MP Autofocus camera board for

Variscite's DART-MX8M

Pic 2: 13MP MIPI CSI-2 i.MX8 Camera Board

TARGETED APPLICATIONS

  • Medical imaging
  • Automation
  • Handheld devices
  • Machine visual inspection systems
  • General purpose HMI solutions
0 项奖励
回复
0 回复数