dtsi for imx8mm single core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dtsi for imx8mm single core

ソリューションへジャンプ
658件の閲覧回数
MB_stek
Contributor III

Hi,

we're using a imx8mm (4x Cortex A53) with Linux. So, our device tree dts includes imx8mm.dtsi (https://elixir.bootlin.com/linux/v6.11/source/arch/arm64/boot/dts/freescale/imx8mm.dtsi) which defines all four A53 cores.

Now our HW department has asked if they can simply replace the imx8mm with a single-core imx8mm (like e.g. the MIMX8MM1CVTKZAA), which are pin compatible, but have only one core. Is it safe to use the same imx8mm.dtsi? If so, will the Linux kernel simply ignore the non-existent other three cores?

Or is there maybe a dedicated .dtsi file for single core?

Or do we need to modify imx8mm.dtsi?

Kind regards,

Markus

ラベル(2)
0 件の賞賛
返信
1 解決策
574件の閲覧回数
vodix
Contributor II

The iMX's u-boot automatically modifies the Linux device tree to disable the number of cores based on the fuses of different chips.

All you need to do is solder the different chips—it's that simple.

I'm using the lf-5.10.72-2.2.3 code for this demonstration to illustrate that this code was available several years ago, around October 2022.

 
lf-5.10.72-2.2.3
 
 
This is code for iMX8MM single core. It deletes 3 core of Linux dts and leave only one.
else if (is_imx8mms() || is_imx8mmsl())
		disable_cpu_nodes(blob, 3);
 
 
#elif defined(CONFIG_IMX8MM)
if (is_imx8mml() || is_imx8mmdl() ||  is_imx8mmsl())
disable_vpu_nodes(blob);

if (is_imx8mmd() || is_imx8mmdl())
disable_cpu_nodes(blob, 2);
else if (is_imx8mms() || is_imx8mmsl())
disable_cpu_nodes(blob, 3);
 

 

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
575件の閲覧回数
vodix
Contributor II

The iMX's u-boot automatically modifies the Linux device tree to disable the number of cores based on the fuses of different chips.

All you need to do is solder the different chips—it's that simple.

I'm using the lf-5.10.72-2.2.3 code for this demonstration to illustrate that this code was available several years ago, around October 2022.

 
lf-5.10.72-2.2.3
 
 
This is code for iMX8MM single core. It deletes 3 core of Linux dts and leave only one.
else if (is_imx8mms() || is_imx8mmsl())
		disable_cpu_nodes(blob, 3);
 
 
#elif defined(CONFIG_IMX8MM)
if (is_imx8mml() || is_imx8mmdl() ||  is_imx8mmsl())
disable_vpu_nodes(blob);

if (is_imx8mmd() || is_imx8mmdl())
disable_cpu_nodes(blob, 2);
else if (is_imx8mms() || is_imx8mmsl())
disable_cpu_nodes(blob, 3);
 

 

0 件の賞賛
返信
476件の閲覧回数
MB_stek
Contributor III

Thanks for the hint with imx u-boot!

We're using mainline u-boot, but this of course helps for inspiration

Kind regards,

Markus

0 件の賞賛
返信
451件の閲覧回数
vodix
Contributor II

Mainline u-boot also has this code.

https://github.com/u-boot/u-boot/blob/master/arch/arm/mach-imx/imx8m/soc.c#L1415

 #elif IS_ENABLED(CONFIG_IMX8MM)
	if (is_imx8mml() || is_imx8mmdl() ||  is_imx8mmsl())
		disable_vpu_nodes(blob);

	if (is_imx8mmd() || is_imx8mmdl())
		disable_cpu_nodes(blob, nodes_path, 2, 4);
	else if (is_imx8mms() || is_imx8mmsl())
		disable_cpu_nodes(blob, nodes_path, 3, 4);
0 件の賞賛
返信
459件の閲覧回数
vodix
Contributor II

This is long-standing code from the NXP iMX BSP.

However, @JorgeCas @ stated that there's no existing code for a single core. We might need to confirm this with @JorgeCas .

0 件の賞賛
返信
440件の閲覧回数
MB_stek
Contributor III

Ok, interesting.

So, in addition to removing the CPU nodes in the DT, one would also need to change the cooling maps node.

Kind regards,

Markus

0 件の賞賛
返信
633件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Leave the 4 cores device tree as it is without remove the unused/non-existent cores in 1 core device is not the best option, could cause from a simple warning to a system hang. 

We do not have a special device tree for single core device but I suggest you remove the non-existent cores in your device tree for the new part number.

Best regards. 

0 件の賞賛
返信
455件の閲覧回数
vodix
Contributor II

@JorgeCas @, could you please comment on your answer to confirm that the code for dynamically modifying the DTB in the NXP IMX BSP is valid and correct

0 件の賞賛
返信
404件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You are right.

U-boot code will change the CPU node status to "disabled" based on CPU information mentioned in fuses.

Just make sure that source code includes this feature.

Best regards.

0 件の賞賛
返信
387件の閲覧回数
kawateb265
Contributor II

@JorgeCas 

disable_cpu_nodes does two things: delete the cpu node and disable the thermal nodes related to the deleted cpu node.
It is not change the CPU node status to "disabled" you mentioned.

 

rc = fdt_del_node(blob, nodeoff);

 

https://github.com/u-boot/u-boot/blob/master/arch/arm/mach-imx/fdt.c

int disable_cpu_nodes(void *blob, const char * const *nodes_path, u32 num_disabled_cores,
		      u32 max_cores)
{
	u32 i = 0;
	int rc;
	int nodeoff;

	if (max_cores == 0 || (num_disabled_cores > (max_cores - 1)))
		return -EINVAL;

	i = max_cores - num_disabled_cores;

	for (; i < max_cores; i++) {
		nodeoff = fdt_path_offset(blob, nodes_path[i]);
		if (nodeoff < 0)
			continue; /* Not found, skip it */

		debug("Found %s node\n", nodes_path[i]);

		rc = fdt_del_node(blob, nodeoff);
		if (rc < 0) {
			printf("Unable to delete node %s, err=%s\n",
			       nodes_path[i], fdt_strerror(rc));
		} else {
			printf("Delete node %s\n", nodes_path[i]);
		}
	}

	disable_thermal_cpu_nodes(blob, num_disabled_cores, max_cores);

	return 0;
}

 

 

 

 

0 件の賞賛
返信
608件の閲覧回数
MB_stek
Contributor III

Thanks for the answer, Jorge!

So, we'll plan to use a dedicated device tree there, based on imx8mm.dtsi with the three missing cores removed as CPU nodes.

Kind regards,

Markus

0 件の賞賛
返信