iMX6Q processor
linux kernel 4.9.88
I will use CTS_B pin as RS485 direction control pin,Could you also help about the dts configuration part?
Sorry that it’s the first time I configure UART.
uart1: serial@02020000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x02020000 0x4000>;
interrupts = <0 26 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6QDL_CLK_UART_IPG>,
<&clks IMX6QDL_CLK_UART_SERIAL>;
clock-names = "ipg", "per";
dmas = <&sdma 25 4 0>, <&sdma 26 4 0>;
dma-names = "rx", "tx";
status = "disabled";
};