[dts] Does "fsl, sai-synchronous-rx" set SAI to I2S Slave?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[dts] Does "fsl, sai-synchronous-rx" set SAI to I2S Slave?

跳至解决方案
2,123 次查看
Takashi_Kashiwagi
Senior Contributor I

Hi Community.

We want to run SAI as Slave of I2S / TDM as follows.

pastedImage_1.png


According to fsl-sai.txt\sound\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel ,

there is an option called “fsl, sai-synchronous-rx”.

Can this option be used when TX_SYNC / TX_BCLK / MCLK is not connected as shown above?

Do I need to connect MCLK?

Best Regards,

T.Kashiwagi

标记 (2)
1 解答
2,011 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kashiwagi

>Can this option be used when TX_SYNC / TX_BCLK / MCLK is not connected as shown above?

yes

>Do I need to connect MCLK?

no

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,012 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kashiwagi

>Can this option be used when TX_SYNC / TX_BCLK / MCLK is not connected as shown above?

yes

>Do I need to connect MCLK?

no

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------