I am trying to the image using mfg tool ,it works and uboot interface comes ,
then i am trying the following commands as given in android user guide
U-Boot > setenv bootcmd boota mmc1 [Load the boot.img from SD card]
U-Boot > setenv bootargs console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32
video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0
consoleblank=0 androidboot.hardware=freescale cma=384M
#[Optional]
U-Boot > saveenv
but when i reboot the board
error comes
unknown command --> boota
How to resolve the issue
Hi sameerarvikar
for environment variables usage please refer to uboot documentation
UBootEnvVariables < DULG < DENX
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------