download the patch of sdma for mach-imx directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

download the patch of sdma for mach-imx directory

485 Views
ganboshi
Contributor II

for linux 2.6.31, the cpu directory plat-mxc have a patch directory sdma for imx25,  but for linux 4.1.15 the cpu directory mach-imx have no patch for sdma,  so where have the sdma  patch for mach-imx i can download. Thanks a lot

0 Kudos
1 Reply

358 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ganbo

compared with old linux, linux 4.1.15 have different sdma code structure

described in Chapter 4 Smart Direct Memory Access (SDMA) API

attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos