does the i.mx7dual board support the msata ssd card on the mini pcie interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does the i.mx7dual board support the msata ssd card on the mini pcie interface?

928 Views
aowiefofoaiwheo
Contributor I

I have bought the I.MX 7 Dual board, i want to use the mSATA ssd on the mini PCIe interface,

but i can't see any ssd information in the dmesg

how can i drive the mSATA ssd?

does the i.mx7 dual board support the mSATA ?

0 Kudos
Reply
2 Replies

776 Views
igorpadykov
NXP Employee
NXP Employee

Hi aowiefo

hardware supports it, however software (linux) may require additional drivers.

Please refer to attached Linux Manual Chapter 40 PCI Express Root Complex Driver

what peripherals were tested.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

776 Views
kevinchan
Contributor I

I have similar question about SSD support on i.MX7.   Could I connect M.2 NVME to mini-PCIE interface on Sabre reference board design?

0 Kudos
Reply