does imx7d support MII interface ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

does imx7d support MII interface ?

跳至解决方案
1,226 次查看
jiangyaqiang
Contributor V

Hi anyone:

I found in RM of imx7d, some MII interface PIN is missing or wrong. 

example:

pastedImage_1.png

TX_CLK should be use as input ,but in RM it's ouput.

and there is no ENET1_TX_EN pin. 

RGMII_TX_CTL is similar to TX_EN, but it used for RGMII only

pastedImage_2.png

Does anyone know the detail of pin assignment for MII interface?

MII interface should contains the following pins:

TXD[0:3] TX_ER TX_CLK/TXC  TX_EN  RXD[0:3] RX_CLK RX RX_XDV COL CRS
标签 (3)
0 项奖励
回复
1 解答
1,100 次查看
art
NXP Employee
NXP Employee

1. There is the typo in the manual regarding the ENETx_TX_CLK signal. Actually, it is input in the MII mode.

2. There is the typo in the manual regarding the RGMIIx_TX_CTL signal. Actually, in MII mode it operates as ENETx_TX_EN.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,101 次查看
art
NXP Employee
NXP Employee

1. There is the typo in the manual regarding the ENETx_TX_CLK signal. Actually, it is input in the MII mode.

2. There is the typo in the manual regarding the RGMIIx_TX_CTL signal. Actually, in MII mode it operates as ENETx_TX_EN.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复