docker in imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

docker in imx6

3,474 次查看
haifeng_jin
Contributor III

hi  i want to run docker at I.mx6,but more errors,can you hlpe me?kernel 4.1.15

INFO[0000] libcontainerd: new containerd process, pid: 292
WARN[0000] containerd: low RLIMIT_NOFILE changing to max current=1024 max=4096
ERRO[0001] Failed to built-in GetDriver graph zfs /var/lib/docker
INFO[0001] Graph migration to content-addressability took 0.00 seconds
WARN[0001] Your kernel does not support cgroup blkio weight
WARN[0001] Your kernel does not support cgroup blkio weight_device
WARN[0001] Your kernel does not support cgroup blkio throttle.read_bps_device
WARN[0001] Your kernel does not support cgroup blkio throttle.write_bps_device
WARN[0001] Your kernel does not support cgroup blkio throttle.read_iops_device
WARN[0001] Your kernel does not support cgroup blkio throttle.write_iops_device
WARN[0001] mountpoint for pids not found
INFO[0001] Loading containers: start.
WARN[0001] Running modprobe bridge br_netfilter failed with message: modprobe: can't change directory to '/lib/modules': No such file or directory
, error: exit status 1
WARN[0001] Running modprobe nf_nat failed with message: `modprobe: can't change directory to '/lib/modules': No such file or directory`, error: exit status 1
WARN[0001] Running modprobe xt_conntrack failed with message: `modprobe: can't change directory to '/lib/modules': No such file or directory`, error: exit status 1
ERRO[0001] could not get initial namespace: no such file or directory
WARN[0001] Could not load necessary modules for IPSEC rules: Running modprobe xfrm_user failed with message: `modprobe: can't change directory to '/lib/modules': No such file or directory`, error: exit status 1
ERRO[0001] failed to set to initial namespace, readlink /proc/286/task/303/ns/net: no such file or directory, initns fd -1: bad file descriptor
INFO[0001] Default bridge (docker0) is assigned with an IP address 172.17.0.0/16. Daemon option --bip can be used to set a preferred IP address
ERRO[0001] failed to set to initial namespace, readlink /proc/286/task/303/ns/net: no such file or directory, initns fd -1: bad file descriptor
Error starting daemon: Error initializing network controller: Error creating default "bridge" network: package not installed

标签 (1)
0 项奖励
回复
1 回复

2,522 次查看
b36401
NXP Employee
NXP Employee

Please try to play with version of docker. Possibly previous one can help.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复