do not enter recovery

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

do not enter recovery

2,027 次查看
donghyunkim
Contributor III

bsp : android_N7.1.1_1.0.0

board : i.MX6qp sabresd

reference document : Android_Frequently_Asked_Questions.pdf (8 How do I enter the Android recovery mode manually?)

"reboot recovery" command does not enter recovery in Android N7.1.1

but, it works in factory reset menu in settings.

and, one strange...

after doing the "reboot ..." command, output "Reset cause: POR" message in u-boot.

is "Reset cause: WDOG" true?

to my recollection, it seems that "Reset cause: WDOG" message in Android gingerbread.

ask for advice.

标签 (2)
0 项奖励
回复
3 回复数

1,779 次查看
marcowang
Contributor II

Hi DongHyun Kim,

Could you please tell me how to set BCB ? Tks

0 项奖励
回复

1,779 次查看
JayTu
NXP Employee
NXP Employee

Factory reset is mandatory but not reboot recovery.

It shows WDOG since reboot is done by watchdog.

0 项奖励
回复

1,779 次查看
donghyunkim
Contributor III

Hi, JayTu.

This problem occurred because did not set BCB.

It's solved.

Thanks!!

0 项奖励
回复