do not enter recovery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

do not enter recovery

1,948 Views
donghyunkim
Contributor III

bsp : android_N7.1.1_1.0.0

board : i.MX6qp sabresd

reference document : Android_Frequently_Asked_Questions.pdf (8 How do I enter the Android recovery mode manually?)

"reboot recovery" command does not enter recovery in Android N7.1.1

but, it works in factory reset menu in settings.

and, one strange...

after doing the "reboot ..." command, output "Reset cause: POR" message in u-boot.

is "Reset cause: WDOG" true?

to my recollection, it seems that "Reset cause: WDOG" message in Android gingerbread.

ask for advice.

Labels (2)
0 Kudos
Reply
3 Replies

1,700 Views
marcowang
Contributor II

Hi DongHyun Kim,

Could you please tell me how to set BCB ? Tks

0 Kudos
Reply

1,700 Views
JayTu
NXP Employee
NXP Employee

Factory reset is mandatory but not reboot recovery.

It shows WDOG since reboot is done by watchdog.

0 Kudos
Reply

1,700 Views
donghyunkim
Contributor III

Hi, JayTu.

This problem occurred because did not set BCB.

It's solved.

Thanks!!

0 Kudos
Reply