do_fetch stuck and notice locks in download/git2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

do_fetch stuck and notice locks in download/git2

1,128 Views
tenmb
Contributor I

Hi Team,

We are building core-image-minimal image for imx8mp-lpddr4-evk board on host system Ubuntu 20.04 and we noticed it is getting stuck always after sometime around 51%.

Approached Tried:  

Tried in different ubuntu systems  -->  result remains same.

Deleted the hole download and build folder and tried --> result remains same.

I noticed same list of repos which is stuck in do_fetch,  is in lock state in download/git2 --> tried to rename it to done and start the build ---> result remains same.

Used this manifest file : https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-honister -m imx-5.15.5-1.0.0.xml

ENV: DISTRO=fsl-imx-wayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b xyz

Build command : bitbake core-image-minimal

Please help.

tenmb_0-1666347028641.png

 

Thank you,

Tenmb

 

0 Kudos
Reply
2 Replies

1,114 Views
joanxie
NXP TechSupport
NXP TechSupport

this is related to your network issue, pls check your firewall or check your proxy settings,the files are too old to upload here, I sent them to you, you put them to the download/git2

0 Kudos
Reply

1,109 Views
tenmb
Contributor I

oe proxy export, fixed this issue.

thanks for your reply.

0 Kudos
Reply