do_fetch stuck and notice locks in download/git2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

do_fetch stuck and notice locks in download/git2

1,035 次查看
tenmb
Contributor I

Hi Team,

We are building core-image-minimal image for imx8mp-lpddr4-evk board on host system Ubuntu 20.04 and we noticed it is getting stuck always after sometime around 51%.

Approached Tried:  

Tried in different ubuntu systems  -->  result remains same.

Deleted the hole download and build folder and tried --> result remains same.

I noticed same list of repos which is stuck in do_fetch,  is in lock state in download/git2 --> tried to rename it to done and start the build ---> result remains same.

Used this manifest file : https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-honister -m imx-5.15.5-1.0.0.xml

ENV: DISTRO=fsl-imx-wayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b xyz

Build command : bitbake core-image-minimal

Please help.

tenmb_0-1666347028641.png

 

Thank you,

Tenmb

 

0 项奖励
回复
2 回复数

1,021 次查看
joanxie
NXP TechSupport
NXP TechSupport

this is related to your network issue, pls check your firewall or check your proxy settings,the files are too old to upload here, I sent them to you, you put them to the download/git2

0 项奖励
回复

1,016 次查看
tenmb
Contributor I

oe proxy export, fixed this issue.

thanks for your reply.

0 项奖励
回复