dm-crypt Error on iMX 6UL EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dm-crypt Error on iMX 6UL EVK

2,039 Views
kanimozhi_t
Contributor V

Hi,

   I'm closely following AN12714 (https://www.nxp.com/docs/en/application-note/AN12714.pdf )for encrypting root filesystem in iMX6UL. And based on my hardware, the only thing I've changed from the provided example is, MACHINE=imx6ulevk (from original imx8mmevk). The build completed without any error but I encounter the following errors in runtime:

root@imx6ulevk:~# grep -B1 -A2 tk- /proc/crypto|grep -v kernel
root@imx6ulevk:~# dmsetup targets
/dev/mapper/control: open failed: No such device
Failure to communicate with kernel device-mapper driver.
Check that device-mapper is available in the kernel.
Incompatible libdevmapper 1.02.140 (2017-05-03) and kernel driver (unknown version).
Command failed
root@imx6ulevk:~# ls -la /dev/mapper/control
crw------- 1 root root 10, 236 Jun 11 12:32 /dev/mapper/control
root@imx6ulevk:~# keyctl add caam_tk seckey "new ecb 16" @s
add_key: No such device

    In the log above, my observation is cryptographic engine is not at all working as grep -B1 -A2 tk- /proc/crypto|grep -v kernel returns nothing and dm-crypt is screwed.

Can you point me what would have gone wrong here? and could you please list steps to debug this?
Labels (5)
0 Kudos
Reply
3 Replies

1,891 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent some comments directly to You.

Regards,

Yuri.

0 Kudos
Reply

1,844 Views
georgiev_influx
Contributor I

Hello , i have MX8MM and have the same problem.

Can you help me, please?

0 Kudos
Reply

1,831 Views
Yuri
NXP Employee
NXP Employee

@georgiev_influx 
Hello,

  Use the recent NXP Linux BSP (L5.4.47). Look at section 9.5 (Disk encryption acceleration)
of "IMX_LINUX_USERS_GUIDE.pdf".

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Regards,
Yuri.

0 Kudos
Reply