device tree source file for jadard JD9365DA-H3 display panel connected to imx8mm core board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

device tree source file for jadard JD9365DA-H3 display panel connected to imx8mm core board

3,434 Views
koteswararao18
Contributor III

Dear team,

am writing Device tree source (dts) file for jadard jd9365d (TFT LCD single chip ) display panel that is connected to freescale imx8mm core board

kernel driver for jd9365d panel is included by referring below  link.  https://github.com/edgeble/kernel/blob/linux-5.10-gen-rkr3.4/drivers/gpu/drm/panel/panel-jadard-jd93...

But dts file code reference for jd9365d panel is added for rockchip core and it can not be referred for writing dts code for imx8mm core board. respective rockchip dts file is given below.

 https://github.com/edgeble/kernel/blob/linux-5.10-gen-rkr3.4/arch/arm64/boot/dts/rockchip/rk3588-edg...

hence requesting to provide some insights / reference dts file of  TFT lcd panel compatible for imx8mm core board as it can be used to write jd9365da panel dts code. 

Attached jd9365d panel document for reference.

Regards

kote

 

Labels (1)
0 Kudos
Reply
3 Replies

2,976 Views
koteswararao18
Contributor III

Hi,

i prepared the device tree file patch along with jd9365da driver patches for review for review. Meanwhile imx8mm board is booted with attached jd9365da panel driver included image but fails to trigger probe() of jadard jd9365da driver . could you please provide insights for further debugging of the issue.?

Regards

koti

0 Kudos
Reply

3,411 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, it will be possible to connect the panel but you have to change your kernel to one supported by nxp, and with well written the dtb.

Regards

0 Kudos
Reply

3,407 Views
koteswararao18
Contributor III
Dear contributor,l

thank you for your reply. Shall i get any reference tft lcd dts file compatible with imx8mm core that is used for writing dts file for jd9365da panel.

Regards
kote
0 Kudos
Reply