/dev/pn544 node is not creating for pn7150 in imx8mm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

/dev/pn544 node is not creating for pn7150 in imx8mm

1,126 Views
PramodKumar
Contributor IV

Dear Team ,

I have followed the https://www.nxp.com/docs/en/application-note/AN11697.pdf  document and did the changes in yocto project kernel 4.14 . Driver is compiled successfully , but the /dev/pn544 node is not creating . If any body implemented it in the same then please suggest me asap .

Regards ,

Pramod

0 Kudos
Reply
1 Reply

1,047 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,PRAMOD,

It seems that PN54x driver is not correctly loaded into linux kernel. So check it according to the following steps, please!

1. Checking device tree

check if driver's name is the same as that of pn54x driver.

2. the probe function of pn54x driver.

Add debug messages in probe function, please!

--checking if probe function abnormally return.

--checking if it normally enter into probe function of pn54x driver.

--checking if pn54x device is normally registered.

Hope above information is helpful for you!

Have a nice day!

B.R,

Weidong

0 Kudos
Reply