/dev/mxc_ipu in IMX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

/dev/mxc_ipu in IMX6Q

1,340件の閲覧回数
joanvicient
Contributor II

Hi,

I have a question regarding the IPU in IMX6 processors: When accessing the IPU via the "/dev/mxc_ipu" kernel device, in case the processor has two IPUs (e.g the IMX6Q or IMX6QP) which IPU is concretely used? I don't see in the ipu_device.c code how a concrete IPU is selected.

Thanks for the help.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,229件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi joan

seems this depends on registration order, most probably first ipu1 then ipu2,

for details one can look on

8. Device Registration and Initialization - Understanding Linux Network… 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信